Managing notifications
Edit notifications as your facility or system evolves. For example, add or remove recipients as staff change, edit schedules if shifts change, create notifications and alarm rules when tags are added or renamed, or when there is a Power Operation Server change.
You can put Notifications Settings into Maintenance Mode. Maintenance mode lets you configure and troubleshoot notifications without notification messages being sent. See Using Maintenance Mode for more information.
After you edit a notification, save your changes.
TIP: If your notification includes a lot of alarm filters and recipients, click Show Selected Items Only to view only the included notification components.
Renaming a notification
- In the Notifications pane, click Manage Notifications.
- In Manage Notifications, click Edit Name.
- Edit the name then click OK.
Duplicating a notification
You can quickly create a new notification by duplicating and renaming an existing one, and then modifying it to meet your needs.
- In the Notifications pane, click Manage Notifications.
- In Manage Notifications, click Duplicate.
- Rename the notification and then click OK.
- From the Notification drop down list, select the notification you duplicated and renamed and then edit it to meet your needs.
The newly-duplicated notification is added to the list of notifications.
Deleting a notification
- In the Notifications pane, click Manage Notifications.
- In Manage Notifications, click
.
- Click Yes to confirm the deletion.